Търсене в енциклопедия

Показване на 381 до 390 от 394 резултати
Uniform corrosion
Metallic corrosion involves the loss of metal at a spot on an exposed surface – ranging from uniform attacks over the entire surface to severe local attacks.
UV water treatment
UV treatment of water is a common method of combating microorganisms. This procedure treats only bacteria that passes the UV bulb and should be regarded as a gatekeeper. This procedure gives no long term protection.
Variable frequency drive
A variable frequency drive is used for adjusting a flow or pressure to the actual demand. It controls the frequency of the electrical power supplied to a pump or a fan. Significant power savings can be achieved when using a VFD.
Vortex impeller
The benefit of a vortex impeller over a channel impeller is the minimised risk of clogging.
Wastewater
Wastewater is a common designation for any water that in one or another way has been affected in quality by human influence.
Water filtration
Filtration of water is a method of combating microorganisms. This procedure treats only bacteria which passes the filter. This method should be regarded as a gatekeeper.
Water flow rate
Required heating capacity and required temperature differential of the medium are relevant when calculating the design water flow rate for a heating system.
Water hammer
Water hammer can cause pipelines to break or induced damage to equipment if the water hammer is severe enough.
Water hammering
Destructive force that relates to the incompressibility of water. The phenomenon often occurs when filling an empty pipe or quickly closing a valve. It often leads to pipe noise or even destruction of pipes, valves etc.
Water hardness
Hard water can be categorized by the ions found in the water. Hardness in water is defined as the presence of multivalent cations.