Търсене в енциклопедия

Показване на 11 до 20 от 43 резултати
Shaft seal
In its most basic form, a shaft seal combines a rotating part with a stationary part.
Shaft seal forces
The parts of the seal inside the pump are subjected to an axial force from the pressure in the pumped liquid.
Shell and tube exchanger
Shell and tube heat exchangers exchange thermal energy from one fluid to another. Because it is characterised by low pressure loss, it is well-suited to air conditioning systems.
SI units
The International System of Units (SI) is the world's most widely used system of measurement, both in everyday commerce and in science
Silicone rubbers
Rubbers are flexible long chain polymers that can be stretched easily to several times their unscratched length and rapidly return to their original dimensions.
Sistema sprinkler ad acqua
I sistemi sprinkler ad acqua utilizzano acqua per la soppressione di incendi negli edifici. La pompa sprinkler antincendio distribuisce acqua mediante un impianto tubario, rilasciandola dagli sprinkler.
Soft pressure build-up
The 'Soft pressure build-up' function ensures a smooth start-up of systems containing empty pipes, for example.
Solenoid valve
Solenoid valves are broadly used for controlling heat or cooling with ON/OFF consumers. An electrical current is turned into a magnetic field, which opens or closes the valve mechanically.
Sources of legionella in commercial buildings other than water systems
Microbacterial growth is not only a problem in hot and cold water systems and cooling towers but also in many other applications in commercial buildings such as water fountains, spas, swimming pools and fruit and vegetable moisturising systems.
Specific density
The specific density of a material or liquid is the term used to describe the unit mass of a material or liquid.