Find case

Показване на 61 до 70 от 234 резултати
Case banner
For brewing beer, only the best pumps are good enough
The 143-year-old brewery Brauerei Zipf is the leading beer brand In Austria. It has reached this dominant position on the basis of its reputation for consistency and due to its dynamic product development strategy.
Forward thinking wins prestigious contract in China
Shenzhen, China: Located in the southern tip of Guangdong province, Shenzhen is the only mainland city that borders on Hong Kong. The city boasts a population of 10 million under its jurisdiction – or about 32 times that 25 years ago, when it was founded and designated as China’s first special economic zone (SEZ).
Fresenius AG is placing all its bets on Grundfos pumps at its group ...
Fresenius AG's main headquarters in Bad Homburg are impressive: the aesthetically appealing architecture, together with the principal materials of glass and steel and the white lime-sand brick, give the impression of bold design, respectability and dynamism.
Front Range Farms
Front Range Farms, located near Fairfield, Montana, encompasses about 2,000 acres of irrigated farmland, owned by Mark Coverdell.
Full control and full automation
BOT Elektrownia Opole S.A. power plant is located 9 kilometres north from the city of Opole, downstream of the Mala Panew River which flows into the Odra River. The existing and planned production facilities cover approximately 290 hectares. This location ensures good opportunities for providing the power supply to the South-Western area of Poland as well as the transfer of energy to other parts of the country and abroad.
Full pump programme supplied to brand-new Tuscan wastewater plant
The new wastewater treatment plant built by V.E.A. in Pietrasanta, Tuscany, uses Grundfos equipment throughout to purify wastewater for reuse at local industries, notably marble and stone works.
Full-line supply brings savings to wine bottling plant
Accolade has installed Grundfos pumps everywhere: hygienic systems, CIP, heating and cooling, water supply, wastewater and more.
Game, set and match to Grundfos Olympic tennis venue well covered by Danish ...
In tennis, you’re allowed two faults before losing the point. In the pump world, faults – and certainly not double faults – are not an option. So when the builders of the Olympic tennis venue in Athens needed a trustworthy and qualified partner for their project, Grundfos was selected as their doubles partner.
Getting it right with a turnkey aeration system
The Valenton wastewater treatment plant in Paris is the second biggest plant in France. Grundfos has designed and installed the aeration systems.
Graasten: Dressing producer prepares for expansions
Danish company Graasten Salater A/S was established in 1947 and has since then produced a variety of food dressings at its headquarters in Graasten, southern Jutland.