Find case

Показване на 31 до 40 от 234 резултати
Case banner
Conserving Bahrain's water resources with Grundfos
Large-scale wastewater pumps from Grundfos help Bahrain conserve its water resources as efficiently as possible.
Constant pressure for machine tool
The Mayfran Company, with more than 1000 employees worldwide and production sites in the United States, Europe and Asia, is one of the leading global manufacturers of conveyor and filtration systems for the metalworking industry.
Controlling vast water volumes at the Dubai Drydocks
Dubai, United Arab Emirates: The Dubai Drydocks have moved on from their early beginnings in 1971 to become one of the leading ship repair yards in the world – and the premier yard between Europe and the Far East.
CR paid for itself after two batches
Agrochemical manufacturer Albaugh Inc. is one of the largest producers of generic herbicide in the US. Albaugh Inc. annually produces some 20 mill. gallons of product around the clock. In their hot water filter wash application, the Missouri-based plant washes 40 batches on a typical day.
CRN Air-Cooled Top solves shaft seal problem at dairy
With a turnover of some EUR 400 million, the Milk Union Hocheifel (MUH) in Germany, is Europe’s largest UHT milk producer (Ultra Heat Temperature) and supplies milk for more than 170 well-known companies.
Custom pump gives higher pressure with less energy
AXA gets 'super' unit for internally cooled machine tools
Customised solution for Switzerland’s largest shopping centre
Einkaufszentrum Glatt is the largest independent shopping centre in Switzerland, and is at the top of the Swiss league in terms of annual turnover (CHF 632.5 million in 2003). Covering more than 43,000 m2, this complex features two department stores, four specialised retail stores, fi ve restaurants, four bars and 90 specialty shops, with parking space for 4,750 cars. The shopping centre employs approximately 1,250 people and was visited by 6,925 million customers in 2003.
Cutting the cost of district heating
Göteborg Energi is a wholly owned subsidiary of Göteborg Kommunala Förvaltnings AB in Gothenburg, Sweden. The company provides district heating, cooling, natural gas, energy services, an optical fibre network and an electricity supply network. The Göteborg Energi district heating network extends over a length of 700 km, and provides heating for more than 90% of all the apartment blocks in Gothenburg.
De Schothorst: Grundfos DME dosing pumps improve standard of poultry research
In the Western European livestock industry, controlling environmental pollution in the form of N and P emissions and ammonia emission is a key issue.
Demand Driven Distribution - great for more than leaks
The Demand Driven Distribution concept has helped drive down energy consumption and maintenance costs for the Dunea water company.