Find case

Показване на 221 до 230 от 234 резултати
Case banner
Two-time award winning CR-H offers water treatment facility significant ...
The Olathe Water Treatment Station #2 in Olathe, KS, agreed to participate in a field test and with the assistance of Grundfos Distributor, Pump & Power of Lenexa, KS, the Multi-Stage CR-H was installed in April, 2009 in a backwash application for membrane wash.
Uni-wing lobe keeps the olive oil flowing
Tucked away in Mendoza, Argentina, the Gabutti family is skilled at producing grape oil, varietal wines, olives in brine and not least extra-virgin olive oil.
Variable-speed immersible pump cuts processing time when grinding
For more than 80 years the Walter AG Group (Tübingen), a company owned by Sandvik AB in Sweden, has been active in the metal processing market, and it is one of the leading companies in the world in the sector. The company’s 2,000 or so employees generate a turnover of 300 million euros, and the product range includes grinding machines and precision tools, as well as software for tool management.
Venceb AS: Special made SP 4 pump
Comparing the technical documentation and the Artesian borehole produced, it became clear that a 6” pump would not fit the borehole and a 4” pump would not meet the specifications. The solution was provided by Grundfos in the form of a custom-made non-standard SP 4” pump.
Verl-Sende: Innovative solutions with Grundfos Digital Dosing
A large number of wastewater treatment plants worldwide have been in operation for many years, and even decades.
Wales Street Primary School uses harvested water to rejuvenate school grounds
Wales Street Primary School, in the inner Melbourne suburb of Thornbury about 7km from Melbourne’s CBD, had a well-grassed oval, and decided to install an underground irrigation system to keep the ground in shape. However, after the system had been installed, the drought arrived and they were unable to use it. Water restrictions meant they couldn’t use mains water, and the oval grass died. Despite several attempts to re-seed it, it developed into a summer dust bowl.
Water saving innovation just what your customers are seeking
Plumbers and plumbing service providers know that millions of homes around Australia feature hot water reticulation systems that waste thousands of litres of water annually – because of the design of their hot water systems.
Werner: Top quality - no charge
Founded in 1956, Wilhelm Werner GmbH in Leverkusen, Germany, is a leading specialist in water treatment systems, especially systems for ultra-pure water.
Whale Pumps Ltd using Grundfos Direct Sensors VFS
Customer had experienced failures (due to debris becoming lodged in the vane bearing) with the paddle wheel flow meters previously being used. They were also looking to reduce the component cost.
When a constant temperature is vital
Copenhagen, Denmark: Throughout the different stages of pharmaceutical production a constant temperature and humidity are extremely important factors.