Find case

Показване на 171 до 180 от 234 резултати
Case banner
Perfect processing with Grundfos
Trevira Neckelmann, a leading textile dye works based in Scandinavia, demands more from their pumps than most manufacturers can handle.
Polish housing society breaks with tradition
THE POJEZIERZE REGION, POLAND: Polish households spend about 12% of their budgets on energy, compared with an average of 4% in the European Union. The over consumption can be attributed to a combination of thermally inefficient buildings and high distribution losses found in Poland. It is estimated that distribution energy losses in some systems amount to 45% compared with a typical figure of 10% in a well-maintained system. Consequently, there is considerable demand for replacement and ...
Porsche meets Grundfos
WALS-SIEZENHEIM, AUSTRIA: Porsche, manufacturer of prestigious cars, chose a Grundfos solution for wastewater management when its existing service centre was greatly expanded.
Port of Brisbane goes green
The Port of Brisbane’s new head office building has become the first in Australia to receive a 5 Star Green Star Office Design v3 Certified Rating from the Green Building Council of Australia (GBCA), and utilises state-of-the-art Grundfos pumps and booster systems to contribute to efficient stormwater harvesting and greywater recycling.
Precision pumping: Getting exactly what you want with Grundfos Digital Dosing
Trevira Neckelmann is a leading textile dye works situated in Silkeborg, Denmark. 750 persons are employed in the 46,500 m² area of buildings in Silkeborg.
Precision through reliability
Competence and quality in linear Electrical Discharge Machining (EDM) technology have a name with a long tradition: Sodick. For nearly three decades, this company has been the only one in the world to develop and build its own EDM machines from scratch. Grundfos pumps play important roles in helping Sodick produce some of the world’s best EDM machines.
Providing professional pump solution for one of Europe’s largest pivot ...
In France some 100 km south of Bordeaux, farmer Jean Claude Briest is the happy owner of one of the largest pivot irrigation system in Europe, and possibly in the world.
Proving energy and cost benefits with CIU 300 BACnet communication modules
As a commitment to reducing greenhouse gas emissions, the British Columbia (BC) provincial government in Canada has provided funding for energy-optimising boiler energy retrofits in their buildings.
Pump Audit identifies 80% savings
Owners of the Mani Brothers 14-story, 232,476 sq. ft. commercial office building in West Hollywood, CA. was having problems with their potable water booster pumps.