Find case

Показване на 151 до 160 от 234 резултати
Case banner
Making things happen in Dubai
Just a century ago Dubai was little more than a desert-strewn landscape where Bedouin tribes roamed the sands.
Mark Lacher's Farm
Originally, Mark used another pump on the site of this field. Poor suction inlet design caused cavitation damage with this high speed (3600 RPM) pump.
Membrane sewage system helps the Great Barrier Reef
Grundfos technology is part of a unique wastewater plant protecting the Great Barrier Reef.
Milko – a modern dairy enterprise with modern-day requirements
Based in northern Sweden, The Milko dairy company develops and markets natural dairy products that satisfy the needs of Swedish consumers for gastronomic experiences.
MLP AG: How cool computers minimise heating costs
The new administration centre of the stock market-listed financial services provider MLP AG in Wiesloch -four low-level buildings with finely wrought, glazed facades -looks every inch like a university campus. Designed as a Corporate University, up to 1,200 MLP advisers gather at the site in Wiesloch every day for training courses and seminars. MLP has 300 business centres around Europe and concentrates on the academic profession. As an independent broker, the financial services provider ...
Modern technology comes to the Royal Mile
The 4-acre Holyrood site incorporates buildings to house the Scottish Parliament debating chamber, committee rooms and office accommodation for 105 Members of the Scottish Parliament (MSPs) and staff, as well as media suites, visitor information facilities, ancillary staff buildings and catering facilities. The Building User Brief for Holyrood stipulated that, wherever possible, the new building should feature the integration of energy-efficient and environmentally conscious design ...
MTRI pumps resistant to aggressive electrolytes: Stainless steel pump head
The ECM process is characterised by high-precision deburring and edge radiusing of metallic components - material is removed precisely from the desired points with no thermal or mechanical stress to the structure of the material.
Multiple pump solutions for fishmeal manufacturer
FF of Denmark is one of the world’s leading manufac­turers of fishmeal and fish oil. On a yearly basis, the company processes some 1⁄2 million ton of raw fish, of which 75% are exported to countries around the world and the remaining 25% are sold in the home market.
Multistage centrifugal pumps for cardboard manufacture
The cardboard manufacturer de Eendracht situated in Appingedam in Holland has been manufacturing cardboard for over 90 years.
New and easy way to manage irrigation systems
Water engineering and specialist sports-turf contractor, MJ Abbot Limited used Grundfos’ new data communication interface when upgrading the sprinkler irrigation system at an exclusive golf links in Northern Ireland. To manage water usage, the club uses the popular TORO SitePro® central control system, which has a standard feature allowing direct integration with pumping systems. However, the integration process could be troublesome at best.