Търсене в енциклопедия

Показване на 1 до 2 от 2 резултати
Kv value
The Kv value expresses the amount of flow in a regulating valve at a given valve position with a pressure loss of 1 bar. The special situation with a fully open valve determines the kvs value.
Kvs value
The Kvs value expresses the amount of flow in a regulating valve at a fully-open valve position and a pressure differential of 1 bar. The Kvs value is a special case of the Kv value, which indicates the flow at a given valve position and a pressure differential of 1 bar.